Changing the Display Colors of a Tool Path

2021-10-06T23:27:25Z

Summary


Details

How can the path colors be changed when displaying a Tool Path? The default colors can be seen in the picture below. The Cut moves are colored light blue, the Engage is yellow, the Retract is white, the Stepover are green, etc.



Solution

Tool Path colors are changed in Machining Method -> Options -> Colors -> Path Display Colors. Any Operation placed in this method will inherit the Path Display Colors that are set.



Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: CAM
Version: V1876
Function: USER_INTERFACE

Ref: 002-8014981

KB Article ID# PL8014981

Contents

SummaryDetails

Associated Components