Solid Edge Colors in 3D PDF are not the same as in model

2021-10-06T23:56:04Z
TRANSLATORS

Summary


Details

The customer is saving their models as 3D PDF to send to their customer. When the customer saves parts that are white in the 3D model, the part looks grey in the 3D PDF.

In Solid Edge one of the components is white colored:

Opening the 3D PDF the white component will be displayed as grey:



Solution

There is no solution to the request to make the 3D PDF display the same as Solid Edge.

The colors in the 3D PDF are identical to those from the Solid Edge face style. Solid Edge does not control the lighting calculation used by the 3D PDF viewer and this is a common issue between various 3D applications and white is an especially difficult color to render "correctly" using the standard lighting algorithm. 

It is possible to define a style in Solid Edge that will appear "more white" by adding some amount of intensity to the emission color (e.g., medium grey).

Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: TRANSLATORS
Version: V219MP10
Function: 3D_PDF

Ref: 002-8014975

KB Article ID# PL8014975

Contents

SummaryDetails

Associated Components

TRANSLATORS: OTHER