Achieving an engage that is linear and circular in fashion.
When selecting an 'Engage Type' of 'Circular' and using the out-of-the-box parameters, the sample path below shows a circular engage only.

Solution
In order to get a linear-circular combination:
- Edit the "Feature Geometry".
- Go to the "Feature" group.
- Edit the "Start Diameter" so it's slightly smaller than the feature "Diameter".
- Select "OK".
- Go to the Non-Cutting Moves.
- Select the "Engage" tab.
- Input "0.000" for the "Minimum Clearance".
Sample path is in the image below.

Notes and References
To change the angle of the linear engage:
- Edit the Non-Cutting Moves.
- Select the 'Overlap' tab.
- Under the Overlap Distance, change the "Angle".

Hardware/Software Configuration
Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: CAM
Version: V1855
Function: HOLE_BOSS_MILL
Ref: 002-8014956