To export an image on the draft to dwg the customer use insert object > 'create new object' > objecttype = paintbrush-image. The imported image gets a border, which they can turn off by right mouse button on the image > properties > tab 'format' > turn off 'show border'. But when exporting this draft to dwg, the image gets a black border again
The draft to export in dwg contains two objects:

Saving in dwg (using the default seacad.ini) and opening the resulting file in autocad you will see:

Solution
The solution is to edit the configuration file "seacad.ini" and change the option Export Object border.
"Export Object border=1" (with default option value 1 means show the border in exported DWG/DXF file.
"Export Object border=0" means hide the border in exported DWG/DXF file.
This option is applicable to all images or OLE objects that exist in a draft file.
Note: These options are applicable at document level not image/OLE object level.
Changing this option the result of the DWG file will be correct:

Hardware/Software Configuration
Platform: INTL64
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: TRANSLATORS
Version: V219MP9
Function: AUTOCAD
Ref: 002-8014952