Solid Edge Changing the zeros Round-Off on a property text does not appear to work

2021-10-06T23:56:02Z
DRAFT

Summary


Details

The user wants to change zeros Round-Off in the Callout Property panel but it does not appear to work.

Below you can see the callout the user wants to change:


Selecting the callout and setting the property Round Off precision "/@" as 1 does not change the result.


 



Solution


The property value is formatted using dimension style parameters - leading/trailing zeros in conjunction with user desired precision '/@'.  In our example, the trailing zeros option is unchecked and thus we do not see the number of zeros change after the decimal point when precision is set to '/@n'.

To enable the 'Trailing' : Go to 'Style' and select Modify -> Units Tab -> check 'Trailing' in the 'Zeros' section then the result will be correct.



Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: SOLID_EDGE
Application: DRAFT
Version: V219MP10
Function: PROPERTY_TEXT

Ref: 002-8014947

KB Article ID# PL8014947

Contents

SummaryDetails

Associated Components

DRAFT: DRAWING_VIEWS