STEP assembly models displayed with no color

2021-10-06T23:56:01Z

Summary


Details

User has a situation where STEP assembly models are displayed with no color when opened in Solid Edge. The edges are displayed but the faces appear missing.  Why? 



Solution

This is due to the STEP file being created with a transparent surface setting in the source software. 
If the option in the STEP SURFACE_STYLE_TRANSPARENT is set to the value of '1' it will cause the models to appear transparent in Solid Edge. 

The solution is to ensure that the STEP file is created without transparent models in the source software or to modify the STEP file so that SURFACE_STYLE_TRANSPARENT value is set to '0'.



Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 10_1803
Product: SOLID_EDGE
Application: TRANSLATORS

Ref: 001-9536924

KB Article ID# PL8014922

Contents

SummaryDetails

Associated Components