Solid Edge Bottom prompt bar not displayed

2021-10-06T23:56:01Z
PART/SHEETMETAL

Summary


Details

When opening Solid Edge, the Prompt Bar at the bottom of the product is not displayed.



Solution

If you are running Solid Edge on a multiple monitor computer, set the machine up so it does not recognize the additional monitors. Then open Solid Edge. This may force the missing sub-window(s) back to the primary screen, at which time you can dock them within Solid Edge. Then close the product, set the machine back to multiple monitors and the prompt bar should still be there.



Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: APPLICATION
Version: V108.0
Function: UI

Ref: 001-9537502

KB Article ID# PL8014911

Contents

SummaryDetails

Associated Components

PART/SHEETMETAL: FEATURES