What controls text spacing with Automatic Coordinate Dimension tool

2021-10-06T23:56:00Z

Summary


Details

What controls the text spacing with Automatic Coordinate Dimension tool



Solution

 This is controlled by the "Text clearance gap" which is a setting in the dimension style. You will click the Style button, which is the button which looks like an upper case slanted A with a much smaller A right next to and above it on the same button. Select Dimension from the list of style types and then pick the actual style you are using. Click on the Modify button and go to the Spacing tab. The item you are looking for is at the top of the list. This is a multiple of the font size. 



Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 764SP1
Product: SOLID_EDGE
Application: DRAFT
Version: V219.0
Function: DIMENSIONS

Ref: 001-9533521

KB Article ID# PL8014909

Contents

SummaryDetails

Associated Components