Importing NX CAM Native Template Parts into Teamcenter

2021-10-06T23:27:25Z

Summary


Details

Knowing the steps involved in importing the template parts moving from version to version in NX.

Solution

Files
  • Open My Teamcenter.
  • Select 'Edit-->Options'.



  • Select the "Search" tab.





  • In the Preferences List..."Search on Keywords"...input "TC_allow" (please see image below).
  • Select "TC_Allow_Longer_ID_Name" from the "Name" column and verify the "Value" is set to "true".

Note: if the "Value" is not "true" … select "Edit" and change it to "true" (see image below).


  • Start the TC Command Prompt from the Windows Start Menu.

  • With the "command prompt" open, type in "set" and select "Enter" on the keyboard.
Note: Verify the following environment variables are set...
  • UGII_BASE_DIR
  • UGII_TMP_DIR
  • UGII_TEMP_DIR
If any of the above do not exist, set them at this time. (please see example in image below).


  • Locate tcin_cam_template_setup.bat in UGII_BASE_DIR\templates\sample
  • Drag tcin_cam_template_setup.bat  from the File Explorer  window to the TC12 Command Prompt window (please see image below)..


  • Place a space after the file name and input -u=username -p=password at the end of the line.
Note: Use your TC logon username and password.


  • Select "Enter" and the import process will begin.






Notes and References


https://docs.plm.automation.siemens.com/tdoc/nx/1872/nx_help/#uid:xid1128418:index_mfggeneral:cust_cam:customize_cust_data_manag
Steps to import NX CAM Template Parts into TC
https://docs.plm.automation.siemens.com/tdoc/nx/1872/nx_help/#uid:id778082

Configuration
"D:\Siemens\NX1872\Siemens\NX1872\MACH\resource\configuration\cam_teamcenter_library.dat"

Template Set
"D:\Siemens\NX1872\Siemens\NX1872\MACH\resource\template_set\cam_teamcenter_general.opt"

Sample Templates
"D:\Siemens\NX1872\Siemens\NX1872\UGII\templates\sample\nxdm_ugs_manufacturing_templates_sample.pax"



Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: NXMANAGER
Version: V1872
Function: DOCUMENTATION

Ref: 002-8014902

KB Article ID# PL8014902

Contents

SummaryDetails

Associated Components