Where are the saved draft callout settings with its texts stored? The saved templates need to be moved over from a previous version to SE 2019. Which file must be copied over to the new system?
Solution
The Callout settings, created by the Callout Properties via Save on the General tab, are stored in the file "DraftCallout.txt".
The file will be found in the Reports folder which is a subfolder of the Solid Edge Installation folder Template. Default location would be: C:\Program Files\Siemens\Solid Edge VERSION\Template\Reports
This "DraftCallout.txt" text file can be copied over to the corresponding SE 2019 Reports folder.
Notes and References
Hardware/Software Configuration
Platform: INTL64
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: DRAFT
Version: V219MP8
Function: ANNOTATIONS
Ref: 001-8423484