Solid Edge AWC 4.1.2 is unable to log in when using a German SE UI

2021-10-06T23:55:57Z
DOC_MANAGEMENT

Summary


Details

The hosted Active Workspace Client (AWC) in Solid Edge does not login when using a German localized UI. Using the Solid Edge English UI and the same login account the hosted AWC will login automatically without issue.



Solution

In this case the Active Workspace Websites Languages were not installed.

After installing the language packs on the AW server the Hosted AWC will open on a localized Solid Edge version using the desired Solid Edge UI language.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V219.0
Function: SEEC

Ref: 001-9525857

KB Article ID# PL8014822

Contents

SummaryDetails

Associated Components

DOC_MANAGEMENT: SEEC