Shaded edges in the model display as thick black lines

2021-10-06T23:27:24Z

Summary


Details

 Shaded edges display as very thick lines on model.



Solution

The reason the shaded edges are displaying as very thick is because the pixel width associated to them is very high.
To resolve this:
1. Select 'File-->Preferences-->Visualization'.
2. Select the 'Line' tab.
3. In the 'Line Width' grouping, select the "Reset to Defaults" button.
Now the pixel range is 1->3 for all line widths. The shaded edges will now display as a normal thickness.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: SYSENG
Version: V12.0.2
Function: VISUALIZATION

Ref: 001-9533397

KB Article ID# PL8014786

Contents

SummaryDetails

Associated Components