When adding a part attribute column to the Check-Mate results tree the values are always empty. What needs to be done to show the values?
Solution
To define and show the part attribute column follow the topics of the documentation under "Validation --> Check-Mate --> Check-Mate customization --> Customization of columns in Check-Mate results".
If no values are shown in the column even though the attribute exists in the part(s), make sure that "Filter Level" is set to "Part".

Now the value(s) of the part attribute should be shown.
Notes and References
https://docs.plm.automation.siemens.com/tdoc/nx/1872/nx_help#uid:xid1128420:index_checkmate:xid615394:xid615396Hardware/Software Configuration
Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: KDA
Version: V12.0.2
Function: VALIDATION
Ref: 002-8014775