How to perform a measurement from the expression editor.

2021-10-06T23:27:24Z

Summary


Details

In PRE-NX11 versions the Measure Distance option is on the Expression Editor dialog. Starting in NX11, how can an expression be created from a measurement?



Solution

To create an expression from a measurement in NX11 and beyond, do the following steps:
 
1) Start the Expression User Interface.

2) Click "New Expression" in left panel. 

3) Type an expression name.

4) Single click the cell under Formula column and then MB3.

5) Select Edit and you will get measure icon.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DESIGN
Version: V12.0.2
Function: EXPRESSION

Ref: 001-9530409

KB Article ID# PL8014742

Contents

SummaryDetails

Associated Components