Drilling - Some features were not cut because a gouge was detected

2021-10-06T23:27:24Z

Summary


Details

Drilling operation. When drill diameter is equal to hole feature diameter, sometimes a message may be given: 'Some features were not cut because a gouge was detected' and the hole is not drilled.



Solution

This may be resolved by making the intol/outtol values larger.In this example the default 0.03mm was changed to 0.1mm



Notes and References

PR 9527080
PR 9346412

Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: CAM
Version: V1847
Function: DRILLING

Ref: 001-9527080

KB Article ID# PL8014695

Contents

SummaryDetails

Associated Components