NX Two of the same components in drawings have different callouts in Parts List.

2021-10-06T23:27:24Z
NX for Design

Summary


Details

2 components have the same name, but it does create 2 separate rows in the parts list, where 1 row was expected with the quantity add-up to 0.002 Kg.


DB_UNITS have set to "kg" as part attribute.
The value quantity=0.001 Kg in the assembly for 2 components. 
Partslist  has only 1 key field: PART_NAME (<W$=@$PART_NAME>). 



Solution

The component attributes are wrongly set for (at least) 1 component. This can be fixed by: 

MB3 -> Properties on the component .. 
  • 1) set Quantity Type=As Required ("A/R") -> Apply, 

  • 2) then return Quantity Type=Number and Quantity=0.001 -> OK


Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 1064
Product: NX
Application: DRAFTING
Version: V1867
Function: TABLES

Ref: 001-9526140

KB Article ID# PL8014693

Contents

SummaryDetails

Associated Components

Drafting