NX 1847 Series critical maintenance software fix is available for download

2021-10-07T00:08:38Z

Summary


Details

Dear Siemens PLM Customer,


We are pleased to inform you that the latest critical maintenance software fix for NX 1847 Series is now available for download from the Siemens PLM Download Server. Please disregard this message if you are on the current NX 1872 series.


     
 Download of NX on Windows 64-bit

 
 
Please use the following steps to download the NX product release and its documentation.
Note: A valid WebKey account is required. 


  • In your browser's address field enter the URL: https://download.industrysoftware.automation.siemens.com/
     
                          Login using your WebKey username and password
     
  • From the Download page, enter "SiemensNX-1867.4100_wntx64" (including the quotes) in the Search field to return a list of links for the Release Letter and the Release Packages.  
       
  • Alternatively the NX product release can be found using file navigator by entering NX into the Product Filter Feature on the left of your browser and then navigating through the NX directory structure as follows:  
    • Expand the "NX Support" folder 
    • Expand the "NX Supported" folder 
    • Expand the "NX 1847 Series" folder 
    • Expand the current release folder (NX 1867.4100)   
       
  • To download the NX product:     
    • Right click on the Release Package files 
    • Select "Save Target As" or "Save Link As" to save the files to your local destination 

  • Note: There are two options to download NX. The first option is recommended for customers running NX 1847 Series and would like to get the latest critical maintenance software fix. To update, download the following file and double click to begin the installation program.  
    • SiemensNX-1867.4100_wntx64_MSP.zip 

  • The second option is recommended for customers who may want to perform their full install of NX 1847 Series using this released critical maintenance software: 
    • SiemensNX-1867.4100_wntx64.zip 

  • Automatic updates will not be available for releases on NX 1847 Series after NX 1867, including NX 1867.4100. Users who are on 1867 with automatic update option turned on will be notified to download and install the 1872 release. If 1867.4100 is preferred, users must download the release from the GTAC Download Server.
 
Please refer to the readme file with the download for instructions on extracting the main zip file.


  • To download the NX documentation:  
    • Expand the "NX Support" folder 
    • Expand the "NX Supported" folder 
    • Expand the "NX 1847 Series" folder 
    • Expand the "NX 1847" folder
    • Expand the "Documentation" folder 
    • Right click on the product documentation link 
    • Select "Save Target As" or "Save Link As" to save the file to your local destination. 
In all cases, please refer to the supplied README file for installation instructions. 


If you encounter any problems during this installation, please contact your local Siemens PLM Software support office.
   
 For current information about NX including News, Events, Case Studies, Software Updates and User Group activities please visit our website by selecting the following links:
 
       http://www.plm.automation.siemens.com/global/en/support/   
       http://support.industrysoftware.automation.siemens.com/gtac.shtml 





Sincerely,


Siemens Product Lifecycle Management Software Inc.
Digital Factory Division



SFB-NX-8014689
Product Information:
  • Product: NX

KB Article ID# PL8014689

Contents

SummaryDetails

Associated Components