Solid Edge How to delete an Inter-Part link in a Solid Edge file

2021-10-06T23:55:55Z
PART/SHEETMETAL

Summary


Details

User found an Inter-Part link in a sheetmetal file, that has to be deleted because they are working with a database.  The Inter-Part link is seen in Design Manager under Show parents:

When opening the file in Solid Edge, there is no link to be seen:



Solution

The Link is not broken, the link is still valid, but the file and the machine, where the link to the assembly points to, is not found, for example, it may be on another network.

The link can nevertheless be deleted:

In Inter-Part Manager select the listed File with Right Mouse Button and then in the Context Menu pick the option: "Break Links"
Although no Links are listed, the "Break Links" command will still break the link to the assembly, so that after saving the file no Parents will be listed In Design Manager.






Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: n/a
Product: SOLID_EDGE
Application: PART/SHEETMETAL
Function: TOOLS

Ref: 002-8014686

KB Article ID# PL8014686

Contents

SummaryDetails

Associated Components

PART/SHEETMETAL: FLAT_PATTERN