Details
How are versions of JT FILE FORMAT in tessUG.config file set.
Solution
JT FILE FORMAT in tessUG.config file is set as shown below:
JtFileFormat = "10"
Here the values can be say "9" or "92" and "92" is another version of "9" say 9.2
similarly the values could be "8" or "81" where "81" is 8.1
Please note if the value is set to say "8", "9" or "10" that means that is highest version of its series.
Hardware/Software Configuration
Platform: INTEL
OS: windows
OS Version: 764sp1
Product: NX
Application: NXMANAGER
Version: V11.0
Function: TRANSLATORS
Ref: 002-8014667