How to Make SEEC part as Reference-Only and Hide in PSE

2021-10-06T23:55:55Z

Summary


Details

How to Make SEEC part as Reference-Only and Hide in PSE

Solution

Two system occurrence properties, Higher Level and Physical Properties, determine whether that occurrence is written to the Teamcenter product structure.


When these two occurrence properties are both set to No, the occurrence is considered a construction/reference. Constructions are not written to the Teamcenter product structure.


Set Teamcenter preference SEEC_Enable_AssemblyConstructions=1 to achieve this.



Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 764
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V219.0
Function: SEEC

Ref: 002-8014663

KB Article ID# PL8014663

Contents

SummaryDetails

Associated Components