Adding a Retract to Clearance Plane Move at Every Step Over Pass when Cutting a Boss

2021-10-06T23:27:24Z

Summary


Details

A CAM program is created to mill a part that is made of a very difficult to machine material. For this reason the part is cut with many small step over passes. A move to the clearance plane is also needed so that the cutter inserts can be easily changed. The tool path might look something like the picture below when complete. How can this tool path be created?



Solution

1. Create a Planar Mill operation and select the Floor Plane.
2. Create the Part Boundary as an Open Boundary Type.


3. Set the Cut Pattern to Standard Drive.



4. Uncheck the Non Cutting Moves -> More -> Collision Check setting.



Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: CAM
Version: V1867
Function: PLANAR_MILLING

Ref: 002-8014651

KB Article ID# PL8014651

Contents

SummaryDetails

Associated Components