Not able to create the. JT from Integrated NX for the assembly

2021-10-06T23:27:24Z

Summary


Details

Not able to create the. JT from Integrated NX for the assembly



Solution

NX does not create JT's for the assembly, unless there is solid data at that level. 
 
UGII_GENERATE_MULTI_CAD_JT=1
If this variable is enabled, then it creates JT dataset for the top assembly, irrespective of whether it has geometry or not.
 
Since there is no geometry at the assembly level, JT Preview/Viewer doesn't display anything.
JT Preview/Viewer tabs are only good for viewing a part JT not assembly JT.
Based on the variable UGII_GENERATE_MULTI_CAD_JT=1, JT dataset got created.
To see the full structure of the assembly you need to send the data to structure manager.
 
Please refer NX Documentation for more details.
 
https://docs.plm.automation.siemens.com/tdoc/nx/12.0.1/nx_help/#uid:xid1162620

Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 10_1607
Product: NX
Application: NXMANAGER
Version: V12.0
Function: FILE_OPEN

Ref: 002-8014641

KB Article ID# PL8014641

Contents

SummaryDetails

Associated Components