How to export an assembly with variant rules applied from Teamcenter

2021-10-06T23:27:24Z

Summary


Details

Apply variant rules to assemblies in Structure Manager. Opening the assembly in NX with the variant rule applied will reflect the applied rule. Is there a way to export an assembly with variant rules applied from Teamcenter?



Solution

Currently there is a below workaround for the same-
 
You can use the functionality "Export Configured UGNX Assembly" available under Structure Manager > Tools > Export Configured NX Assembly.
 
To enable this functionality, set "TC_ExportConfigUGNXAssembly" site preference to "TRUE" and applied a variant configuration to existing structure in Structure Manager.
 
The structure, as configured in Structure Manager, was exported and maintained in a native format (i.e., only those components that were shown in Structure Manager were exported).  On opening the assembly in native NX, the Assembly Navigator shows all missing components and NX complains that it can't find the missing components (in TCIN these components would have been suppressed if the structure had been sent to NX due to effectivity or variants).  This is because in native NX, the structure is being read from the assembly part file.  The Export Configured NX Assembly utility utilizes ug_clone - it does not make changes to the part files internal assembly structure when the assembly is exported to its native format.

Notes and References

9366762

Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: XP64_SP2
Product: NX
Application: NXMANAGER
Version: V12.0.2
Function: CLONE_EXPORT

Ref: 002-8014635

KB Article ID# PL8014635

Contents

SummaryDetails

Associated Components