How to verify which standard (ISO or JIS, etc.) is set for "Hole" Feature.

2021-10-06T23:27:23Z

Summary


Details

How to verify which standard (ISO or JIS, etc.) is set for "Hole" Feature.



Solution

1. In the kits of NX distribution like, "C:\Siemens\NX11\ugii\modeling_standards" there is a xml file named "nx502_Threaded_Hole_Standard.xml".
2. In this file resides the column of "ScrewStandard"(Refer the xml in Excel format).
3. In the file for each mentioned "Standard", respective standard type can be seen in the ScrewStandard column .
 
So, if you open the nx502_Threaded_Hole_Standard.xml" in Excel you can clearly see the Screw Standard, refer below snap for your reference-



Notes and References

9514407

Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: XP64_SP2
Product: NX
Application: DESIGN
Version: V11.0.2
Function: FEATURE_MODEL

Ref: 002-8014605

KB Article ID# PL8014605

Contents

SummaryDetails

Associated Components