In Structure Manager Graphics environment assembly features not synchronized

2021-10-06T23:55:53Z

Summary


Details

Assembly features are not synchronized to Teamcenter although the Teamcenter preference

SEEC_Image_Generate_3D = 1SEEC_Image_Generate_Asm_3D = TRUE 

In the local SEEC Cache we can see that the part JT is created but there are no JT override files for the assembly features. 



Solution

Check the following registry key: 

BOMUPDATE_INCREMENTAL
 
The default value for this registry key should be "1"

Reset the registry key if it says "0"



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: suse
OS Version: 11.1
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V110MP12
Function: SEEC

Ref: 001-9512740

KB Article ID# PL8014580

Contents

SummaryDetails

Associated Components