Can you convert an old Hole Table to the New Hole Table format?

2021-10-06T23:55:53Z

Summary


Details

Can a Hole Table prior to Solid Edge ST10 be converted to the new SE 2019 Hole Table format in Draft?



Solution

The short answer is No and it cannot and will not be changed or modified to do so. However, what can be done if you wish to have the old format of Hole Table in SE 2019 is to do the following:

- While in the Draft environment...
- Click the "Customize" button on the Quick Access Bar at the top of the Solid Edge application window
- Click "All Commands" option from the "Choose commands from:" drop list
- From the "Quick Access" tab, select "Legacy Hole Table" from the list, then "Add" so that it appears on the Quick Access toolbar
- You can now use the old method for Hole Table used in ST9 and prior.



Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 10_1809
Product: SOLID_EDGE
Application: DRAFT
Version: V219MP6
Function: TABLES

Ref: 001-9515080

KB Article ID# PL8014568

Contents

SummaryDetails

Associated Components