Solid Edge Solid Edge 2019 - Maintenance Pack 8 Announcement

2021-10-07T00:10:01Z
SE_BETA SE_TSS DOC_MANAGEMENT FLOEFD 3D-SKETCH SIMULATION Teamcenter Share TECH_PUB ASSEMBLY APPLICATION PART/SHEETMETAL TRANSLATORS DRAFT SETUP

Summary


Details

June 24, 2019
 
Dear Solid Edge Customer: 
 
Solid Edge 2019 Maintenance Pack 8 is now available for download.
 
Sincerely,
The Solid Edge Team 
 
============
Release Notes:
============
 
Solid Edge 2019 Maintenance Packs are delivered using Microsoft Installer (MSI) technology.
 
Microsoft Windows 10 releases Feature Updates every six months. Microsoft does not use Windows 10 Feature Updates as an avenue to deliver security-related patches. All quality-related patches, including security and reliability hot-fixes, will continue to be delivered outside of this Feature Update process. Therefore, if your production use of Solid Edge was negatively impacted as a result of the last Microsoft Windows 10 Feature Update, you should consider configuring your Windows 10 machines to delay the deployment of Windows 10 Feature Updates. Configuring your Windows 10 machines by moving the machines into the "Semi-Annual Channel" servicing channel will delay the installation of Feature Updates for approximately four months following the initial release. During this time, you and your IT organization will have the opportunity to review the suitably of the Feature Update, including determining any negative impact, upon the applications that you use in your production environment, such as Solid Edge. This four-month window of time between Microsoft initially releasing the Feature Update to targeted machines and releasing the Feature Update for general deployment to the enterprise will also provide our development team time to review and react to changes introduced by Windows 10 Feature Updates, thereby helping keep you as productive as possible.
 
=====================
Maintenance Pack Version:
=====================
 
Solid Edge 2019 MP8
Version: 219.00.08.04
 
================
Download Location:
================
 
Solid Edge 2019 Maintenance Packs can be downloaded from:
 
   https://download.industrysoftware.automation.siemens.com/solid_edge/2019/Maintenance_Packs/
 
==========
Installation:
==========
 
  • MSI Product Updates can be applied on top of the base release and or existing Product Update with a lesser version.
  • MSI Product Updates are all-inclusive, i.e. fixes delivered in MP3 include all fixes delivered in MP1 and MP2.
  • MSI Product Updates calculate free disk space before installing. Please be patient.
  • MSI Product Updates are uninstalled via the Control Panel (Uninstall a program –> View installed updates -> Uninstall).
  • MSI Product Updates can be uninstalled without having to remove the base Solid Edge product.
  • Uninstalling an MSI Product Update will restore the installation to the state before the Product Update was applied.
  • When uninstalling, the original source media must be available to allow the recovery of previous file versions.
  • The current MSI Product Update will be the only Update listed and available for uninstallation. 
  • After the current Product Update is uninstalled the previous Product Update will become the current Update.
  • .zip files delivered with this MP such as SEECAdministratorV219.zip are complete product setups. Therefore, existing versions of these installs must be removed using Uninstall a program from the Control Panel before installing the new version.
 
===============
E-mail Notification: 
===============
 
To receive direct e-mail notifications for new Solid Edge Maintenance Packs, subscribe to the SFBmail notification.
 
For details on initiating your email subscription navigate to: 
https://www.plm.automation.siemens.com/global/en/support/email-subscription.html
 
============================================
This Maintenance Pack addresses the following PRs:
============================================
 
===General===
PR 8560446: ALT key causes "Attach Locale resources" Error in Korean UI (PR9283547)
PR 9492059: Open 3d models with read-only access when running Solid Edge in viewer mode
 
===Assembly=== 
PR 9183972: Solid Edge crashes when opening a .jt
PR 9347654: Added safety checks for some assembly crashlog aborts
PR 9386843: Deleting parts causes wire path to be deleted, which leads to an abort 
PR 9465131: Scroll wheel zoom in/out view manipulation is really slow 
PR 9466670: Can't update model to Keyshot in SE2019 MP6
PR 9498580: Manual draw command of explode lines not working correctly
PR 9502953: Solid Edge crashing when opening wire harness assembly
 
===Draft=== 
PR 9446381: When the drawing is inactivated and opened, the balloons become "NA"
PR 9494273: Leader annotation behave not correctly by moving leader line
 
===Part/Profile/Sheet Metal===
PR 9313757: Standard Parts Part finder Error Unit bar 100 Faktor to high as original value
PR 9383904: issue using include and colinear to drive a normal cutout
PR 9455273: 'Save As' followed by an additional 'Save' leads into an abort 
PR 9497664: Profile Error Assistant not displaying
PR 8411799: Unable to extend V13.00 category with new master parts
 
===Translators===
PR 9366800: SW Data Migration: Missing File Error 
PR 9243839: Solid Edge crashes when opening a specific NX file
PR 9325596: Dimension scales are incorrect when multiple DV scales are exported
PR 9328958: Opening DXF files is very slow
 
===Design Manager===
PR 8417497: Design Manager missing Property Manager in non-Insight mode
PR 9498880: Preview pane causes errors with scrolling and open files that are in insight 
 
===Data Management===
PR 9497402: SE PDM problem after MP7 installation
 
===Teamcenter Integration for Solid Edge===
PR 9397674: Standard Parts Item name is filled with Item ID instead of configured Project Name
PR 9429418: Error message when open read only SE files from Teamcenter
PR 9432227: Assembly files marked dirty after updating to SE 2019 
PR 9472063: Inconsistent behavior driven reference during delete workflow
PR 9472132: ATTI crashing while import data in manage mode
PR 8417685: BOM line not found error during upload
PR 9486286: Download to cache will change BOM synchronization option
PR 9498560: SEEC_Synchronize_ItemNumbers does not work with Method=3 and Driven References
PR 9352385: Construction Components not synced to TC for an AP Assembly
PR 9432015: When DFT of ASM has independent - view of child PAR, SESE refreshes L - Panel incorrectly
PR 9433947: Revise/Save As on SESE fails when TC side BVR of Sub- Assembly is updated after upload.
PR 9435448: On SESE, BOM of the R-Panel is overridden when Where Used after Set Action 
PR 9487158: Very low open performance of complex draft.
PR 9507197: Adjustable assembly recognition trouble using SEEC API CreateBOMandRelations
PR 9505900: SEEC not listed when trying to borrow licenses

SFB-SOLID_EDGE-8014556
Product Information:
  • Product: SOLID_EDGE

KB Article ID# PL8014556

Contents

SummaryDetails

Associated Components

SE_BETA