NX Plunge Milling gives error: "Matrix is non orthonormal"

2021-10-06T23:27:23Z
NX for Manufacturing

Summary


Details

Case specific problem: Generating a Plunge Milling operation gives error: "Matrix is non orthonormal", and an empty tool path is generated.



Solution

This was found to be due to the holder definition. In this case, reducing the corner radius on a holder segment to be less than the segment length worked around the problem.



Notes and References

PR 9516965

Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: CAM
Version: V12.0.2
Function: PLUNGE_MILLING

Ref: 001-9516965

KB Article ID# PL8014511

Contents

SummaryDetails

Associated Components

Manufacturing General