Tecnomatix How to use the v14.1.2 automatic project attributes

2021-10-07T00:01:48Z
Process Simulate

Summary


Details

In Tecnomatix 14.1.2, there is a new feature for automatic project attributes for the following:

- movies
- images
- motion volume
- robot macros
- spss 

The documentation says it uses the same mechanism as TuneCellPath definition, but user could not get it to work. 

Please provide steps to utilize this new feature. 



Solution

The Path definition for the other attribute definitions is either relative to sysroot (must have leading hash "#"), or an absolute path string. The TuneCellsPath is hardcoded to be under sysroot, so no "#" was required.

And only MotionVolumesFolderPath must be below the system root, for the other 4 it is not compulsory. 

- ImageFolderPath
- MovieFolderPath
- RobotMacrosFolderPath
- MotionVolumesFolderPath
- SpssFolderPath 



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: n/a
Product: TECNOMATIX
Application: PROCESS_SIMULAT
Version: V14.1.2
Function: INFORMATION

Ref: 001-9513972

KB Article ID# PL8014507

Contents

SummaryDetails

Associated Components

Process Simulate User Interface