Solid Edge Want to place pattern around existing occurrence.

2021-10-06T23:55:52Z
PART/SHEETMETAL

Summary


Details

Have a hole in the middle of a part and want to place a rectangular pattern that extends in both directions from the hole. 



Solution

Place the rectangle relative to the hole so it makes sense for how you want the pattern and then use the Reference Point step to select the point in the pattern that is coincident with the existing hole.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: PART/SHEETMETAL
Version: V219MP7
Function: FEATURES

Ref: 001-9517113

KB Article ID# PL8014497

Contents

SummaryDetails

Associated Components

PART/SHEETMETAL: FLAT_PATTERN