Saving an NX item in Teamcenter as a different NX Item Type

2021-10-06T23:27:23Z

Summary


Details

The ItemType is not available in the list during a 'Save As New Item Type' command from NX. 
This Item Type is available in Teamcenter when the user goes to 'File-->New-->Item', but not when the NX user goes to 'File-->Save-->Save As New Item Type'.



Solution

ItemTypes that have required properties with no initial value will not be available in the NX 'Save As New Item Type' list. This is as designed. NX cannot use those ItemTypes, as they would create Items that may have required properties that are <empty> or null.
To workaround the issue, set an initial value for all required properties for this needed ItemType in BMIDE. Then save the template and deploy. If the ItemType has a default initial value for all required properties and is available to the user's group/role, it should start being available in the Item Type list in NX for the 'Save As New Item Type' command.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: NXMANAGER
Version: V1926
Function: FILE_SAVE_AS

Ref: 001-9514200

KB Article ID# PL8014495

Contents

SummaryDetails

Associated Components