Solid Edge Problem with Clone Component of an Adjustable Part

2021-10-06T23:55:51Z
ASSEMBLY

Summary


Details

In Solid Edge 2019 assembly environment and earlier you can select an adjustable part from the Pathfinder and then clone that Part without any problem, but when finishing and the part is added to the assembly, one can see that the adjustable parts do not have the required dimension that was defined, so they will have the size of the original part.  Furthermore, you cannot select the adjustable part after having clicked on the Clone Component command.

Solution

It was never planned to clone adjustable parts.  It is not possible to selected adjustable parts within the Clone Component command, however they could be still be selected from the Pathfinder even though this should not have been allowed.

In Solid Edge 2020 this problem has now been resolved - it is no longer to allowed select or use adjustable Parts to clone those components.

Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: n/a
Product: SOLID_EDGE
Application: ASSEMBLY
Version: V219.0
Function: COMPONENTS

Ref: 002-8014482

KB Article ID# PL8014482

Contents

SummaryDetails

Associated Components

ASSEMBLY: ANNOTATIONS/DIMENSIONS