Details
Where is the setting [Menu > Preferences > User Interface > Options > Default Presentation of Dialog Content] is stored?
Solution
The setting "Default Presentation of Dialog Content" is stored in the user.mtx file and is also saved as part of a role. The Essentials role will set it to Less and the Advanced role will set it to More.
Hardware/Software Configuration
Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: GATEWAY
Version: V12.0.2
Function: PREFERENCES
Ref: 002-8014472