A part has multiple threaded holes. These holes have different
Thread Pitch values. Since the tool only cuts one thread at a time is it possible to mill all of these threads
using the same tool? Only one tool will need to be setup on the NC machine if possible.

Solution
1. The
(P) Pitch setting for the
Thread Mill Tool is set to a value and the
Form Type is set to
Metric.

2. When the
Thread Mill operations are generated with this tool the message below is displayed.

3. This occurs because the specified tool
Pitch does not match the
Pitch in every operation.

4. Change the
Thread Mill Form Type to the
Partial Profile 60 option. With this
Form Type selected the
(P) Pitch will be entered as the maximum pitch size that the tool is able to cut.

5. When the operations are generated no errors are reported and all paths are correctly cut. Setting the
(FL) Flute Length to match the
(P) Pitch will automatically machine the thread using a
Continuous Cut pattern.
Hardware/Software Configuration
Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: CAM
Version: V1867
Function: THREAD_MILL
Ref: 002-8014459