Solid Edge Physical Properties in Solid Edge to import to Teamcenter

2021-10-06T23:55:49Z
PART/SHEETMETAL

Summary


Details

Is it possible to add the physical properties (e.g. Mass) to the custom property list or to the data preparation utility template?  Alternatively is there a way to import these physical properties in Solid Edge to Teamcenter using Add to Teamcenter utility too?



Solution

If the Solid Edge Mass is mapped (master=cad)  it will synchronize to Teamcenter during an Add To Teamcenter bulkload.

There is no need to have this in the data prep xlsm, since these attributes are calculated by Solid Edge.  The physical properties are CAD only attributes and retrieved from the Solid Edge Material table.  You can still synchronize to add Material to the data prep xlsm to make it visible in Teamcenter if wished but  you need to take care.  Ultimately physical properties are managed by Solid Edge.





Notes and References

See also:

FAQ 001-7918813 - Creating a common material library for all Solid Edge users

https://solutions.industrysoftware.automation.siemens.com/view.php?sort=desc&q=SEEC+material&dt=faq&file_type=html&i=001-7918813&k=0&o=0

FAQ 002-7002830 - Managing Solid Edge Physical Properties with SEEC

https://solutions.industrysoftware.automation.siemens.com/view.php?sort=desc&q=SEEC+material&dt=faq&file_type=html&i=002-7002830&k=1&o=0


FAQ 001-2103263 - Solid Edge Material property mapping with TC

https://solutions.industrysoftware.automation.siemens.com/view.php?sort=desc&q=SEEC+material&dt=faq&file_type=html&i=001-2103263&k=4&o=0

Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V219MP7
Function: DATA_PREP

Ref: 002-8014441

KB Article ID# PL8014441

Contents

SummaryDetails

Associated Components

PART/SHEETMETAL: FEATURES