The red exclamation mark in the drawing view properties

2021-10-06T23:55:48Z

Summary


Details

If you see the red exclamation mark in the drawing view properties on the Parts List tab, you can right-mouse-click on the solid body and get more information.  If it states that the fill style used in the part is not present in the draft and you do not want to use the fill style from the part, the red exclamation mark does not go away.

Solution

In order to get rid of the red exclamation mark saying that the fill style from the part is not present in the draft,  you need to first deselect the option 'Derive fill style from part' and then force an update on the drawing view using CTRL + SHIFT + Update view.

Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 764sp1
Product: SOLID_EDGE
Application: DRAFT
Function: DRAWING_VIEWS

Ref: 002-8014389

KB Article ID# PL8014389

Contents

SummaryDetails

Associated Components