How to assign time to motion sequence in an operation, with automatic speed calculation?
How to create a time-based operation?
Solution
Edit speed form "default value for speed" to "Auto Calculate", which means the speed is calculated automatically:

For this select
MB3 on the value-cell and choose "Auto Calculate" from dropdown list.
Then you can set the time, and the speed is calculated accordingly.
Notes and References
Tdoc:
Mechatronics Concept Designer >
- Assigning, changing and controlling properties >
- Creating time-based and event-based behaviors >
- Create a time-based operation.
https://docs.plm.automation.siemens.com/tdoc/nx/12.0.2/nx_help/#uid:index_mechatronics:xid896264:id1101473:id1109426Hardware/Software Configuration
Platform: INTEL
OS: windows
OS Version: 1064
Product: NX
Application: MECHATRONICS
Version: V12.0.2
Function: PROCEDURE
Ref: 001-9504393