The Time column in the operation navigator shows a total time for the operation, including the time for rapid moves. What does the software use for a rapid motion rate for these calculations?
Solution
This is a property of the machine in the setup, and does include the default GENERIC_MACHINE.
Change the ONT to the Machine Tool view, right click the machine, and pick Edit. Look in the Time Estimates group for the setting:
Hardware/Software Configuration
Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: CAM
Version: V12.0.2
Function: USER_INTERFACE
Ref: 002-8014274