Manually uninstalling Solid Edge after failed uninstall

2021-10-06T23:55:45Z

Summary


Details

When attempting to uninstall Solid Edge, the uninstall fails and Solid Edge is not fully uninstalled. How to clean up and manually finish uninstalling Solid Edge after a failed uninstall?

Solution

If you have issues with uninstalling Solid Edge through "Add and Remove Programs" then you will need to perform a manual uninstall using the following steps:

1. Manually delete the Solid Edge program folders in the Solid Edge install locations, typically found under "C:\Program Files\Siemens\" e.g. "C:\Program Files\Siemens\Solid Edge 2019\".

2. Manually delete the Solid Edge user preference folder under %APPDATA% e.g. "%APPDATA%\Siemens\Solid Edge".

3. Manually clean up the registry by deleting any Solid Edge registry entries in the following locations:


  • HKEY_CURRENT_USER\Software\Siemens\Solid Edge
  • HKEY_CURRENT_USER\Software\Unigraphics Solutions\Solid Edge 
  • HKEY_LOCAL_MACHINE\Software\Siemens\Solid Edge
  • HKEY_LOCAL_MACHINE\Software\Unigraphics Solutions\Solid Edge 
  • HKEY_LOCAL_MACHINE\Software\Wow6432Node\Siemens\Solid Edge
  • HKEY_LOCAL_MACHINE\Software\Wow6432Node\Unigraphics Solutions\Solid Edge 

Note: There are still registry entries created with Solid Edge 2019 that refer to the previous pre- Solid Edge 2019 nomenclature of "Unigraphics Solutions".

4. Reboot the workstation.

Solid Edge should now be completely uninstalled and ready to reinstall Solid Edge.

Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 1064
Product: SOLID_EDGE
Application: SETUP
Version: V219.0
Function: INSTALL

Ref: 002-8014233

KB Article ID# PL8014233

Contents

SummaryDetails

Associated Components