NX Wrong output using File => Plot in NX with RASTER/RTL (PCL) models

2021-10-06T23:27:22Z
NX System Administration

Summary


Details

Starting with NX 12 in some cases the output of the File => Plot command in NX causes distorted results when the used model is defined as RASTER/RTL. 
This also might happen when you try to use RASTER/RTL to communicate with a PCL Printer.

Solution

Copy the file ...\NX11\NXPLOT\bin\win_mft.dll to ...\NX11\NXPLOT\bin

The file "win_mft.dll" can be downloaded from following link:

https://www.sdicgm.com/downloads/siemens/win_mft_nx11.zip

Notes and References

https://www.sdicgm.com/downloads/siemens/win_mft_nx11.zip

Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: GATEWAY
Version: V12.0.2
Function: PLOTTING

Ref: 002-8014222

KB Article ID# PL8014222

Contents

SummaryDetails

Associated Components

Plotting