Solid Edge Flat pattern flips after adding feature

2021-10-06T23:55:43Z
PART/SHEETMETAL

Summary


Details

After un-suppressing a Chamfer, the previous Flat Pattern flips from the already selected orientation.



Solution

The selected X-axis has been removed from the Flat pattern.  The Chamfer was placed on the selected edge. This is also reported by the grey arrow in the PathFinder, with the informational message "An edge/vertex has been removed and the flat pattern orientation may have changed. The flat pattern should be redefined". 

This causes Solid Edge to return to a default position. 

Simply re-create the Flat Pattern and it will work again.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 10_1803
Product: SOLID_EDGE
Application: PART/SHEETMETAL
Version: V219.0
Function: FLAT_PATTERN

Ref: 001-9499942

KB Article ID# PL8014219

Contents

SummaryDetails

Associated Components

PART/SHEETMETAL: FLAT_PATTERN