Simulation: highlighting/locating solving error location

2021-10-06T23:55:43Z

Summary


Details

In Solid Edge Simulation when solving a study an error can occur due to e.g. a wrong mesh.  In the F06 log dialog box the element number or grid point (node) will be given.  In the study the grid point or element numbers are not shown and you cannot search for them.  So there is no ability to locate the location of the problem.  Is there any solution to this?



Solution

In Solid Edge 2020 you can select the Element ID in the drop-down of 'Mesh quality', then 'zoom fit', and the bad quality element will be shown. 



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 1064
Product: SOLID_EDGE
Application: SIMULATION
Version: V219MP6
Function: MESH

Ref: 001-9499381

KB Article ID# PL8014213

Contents

SummaryDetails

Associated Components