NX How to add Sheet Metal features after the Flat Pattern feature?

2021-10-06T23:27:22Z
NX for Design

Summary


Details

Adding a new Sheet Metal feature is adding the feature before theFlat Pattern feature. How can a feature be added after the FlatPattern feature?


Solution

The new NX12 flat pattern features has the option for "Fix at current timestamp", toggling this option ON and adding a new Sheet Metal feature, that feature will be added after the Flat Pattern feature.
If the flat pattern feature is a Pre-NX12 flat pattern it will nothave the "Fix at current timestamp" option.
The Pre-NX12 Flat Pattern can be converted to the new NX12 FlatPattern feature by using the "Renew Feature" function.
Menu --> Edit --> Feature --> Renew Feature
Refer to the NX12 documentation and What's new in NX12 for more information on Renew Feature.


Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 1064
Product: NX
Application: NX_SHEET_METAL
Version: V1859
Function: FLAT_PATTERN

Ref: 001-9499192

KB Article ID# PL8014212

Contents

SummaryDetails

Associated Components

Sheet Metal