Countersink hole outer lines missing in DXF exported Flat Pattern

2021-10-06T23:55:43Z

Summary


Details

The outer lines of countersink holes are missing in a DXF file exported Flat Pattern



Solution

Please check in the "Save as Flat" Options the Layer Tab if in the column SE Features the "Complex Hole" is activated for the "Export to DXF".

This is need to get the Countersink holes completely translated.

For more details please see our online documentation:

http://docs.plm.automation.siemens.com/tdoc/se/2019/se_help/#uid:saveasflat4d



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 1064
Product: SOLID_EDGE
Application: PART/SHEETMETAL
Version: V219.0
Function: SAVE_AS_FLAT

Ref: 001-9498556

KB Article ID# PL8014211

Contents

SummaryDetails

Associated Components