Symbolica Expressions are in use and cannot be deleted

2021-10-06T23:27:22Z
Symbolica

Summary


Details

When deleting an expression, the expression will not delete and the following message is given: 
Expression is still in use. 

How can it be determined where an expression is being used so it can be deleted?



Solution

To see a list of references or where the expression is used, perform the following:
In the Expressions dialog, highlight an expression, 'MouseButton3-->List References'.
An Information window will appear reporting where the expression is being referenced. 
Some examples of where an expression can be used is by another expression, a part family spreadsheet, or a cell in a Tabular Note.
Once this reference is removed, try deleting the expression again. 



Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: n/a
Product: NX
Application: DESIGN
Version: V12.0.2
Function: EXPRESSION

Ref: 001-9496235

KB Article ID# PL8014172

Contents

SummaryDetails

Associated Components

Symbolica