May 20, 2019 Dear Solid Edge Customer: Solid Edge 2019 Maintenance Pack 7 is now available for download.
Sincerely,
The Solid Edge Team ============
Release Notes:============
Solid Edge 2019 Maintenance Packs are delivered using Microsoft Installer (MSI) technology.
Microsoft Windows 10 releases Feature Updates every six months. Microsoft does not use Windows 10 Feature Updates as an avenue to deliver security-related patches. All quality-related patches, including security and reliability hot-fixes, will continue to be delivered outside of this Feature Update process. Therefore, if your production use of Solid Edge was negatively impacted as a result of the last Microsoft Windows 10 Feature Update, you should consider configuring your Windows 10 machines to delay the deployment of Windows 10 Feature Updates. Configuring your Windows 10 machines by moving the machines into the "Semi-Annual Channel" servicing channel will delay the installation of Feature Updates for approximately four months following the initial release. During this time, you and your IT organization will have the opportunity to review the suitably of the Feature Update, including determining any negative impact, upon the applications that you use in your production environment, such as Solid Edge. This four-month window of time between Microsoft initially releasing the Feature Update to targeted machines and releasing the Feature Update for general deployment to the enterprise will also provide our development team time to review and react to changes introduced by Windows 10 Feature Updates, thereby helping keep you as productive as possible.
=====================
Maintenance Pack Version:=====================
Solid Edge 2019 MP7
Version
: 219.00.07.04 ================
Download Location:================
Solid Edge 2019 Maintenance Packs can be downloaded from:
https://download.industrysoftware.automation.siemens.com/solid_edge/2019/Maintenance_Packs/ ==========
Installation:==========
- MSI Product Updates can be applied on top of the base release and or existing Product Update with a lesser version.
- MSI Product Updates are all-inclusive, i.e. fixes delivered in MP3 include all fixes delivered in MP1 and MP2.
- MSI Product Updates calculate free disk space before installing. Please be patient.
- MSI Product Updates are uninstalled via the Control Panel (Uninstall a program –> View installed updates -> Uninstall).
- MSI Product Updates can be uninstalled without having to remove the base Solid Edge product.
- Uninstalling an MSI Product Update will restore the installation to the state before the Product Update was applied.
- When uninstalling, the original source media must be available to allow the recovery of previous file versions.
- The current MSI Product Update will be the only Update listed and available for uninstallation.
- After the current Product Update is uninstalled the previous Product Update will become the current Update.
- .zip files delivered with this MP such as SEECAdministratorV219.zip are complete product setups. Therefore, existing versions of these installs must be removed using Uninstall a program from the Control Panel before installing the new version.
===============
E-mail Notification: ===============
To receive direct e-mail notifications for new Solid Edge Maintenance Packs, subscribe to the SFBmail notification.
For details on initiating your email subscription navigate to:
https://www.plm.automation.siemens.com/global/en/support/email-subscription.html ============================================
This Maintenance Pack addresses the following PRs:============================================
===Assembly=== PR 9321519: Assembly components not visible on the screen or in Pathfinder
PR 9380800: Wire Harness license is being checked out even though user is not in it
PR 9385677: Unable to recognize pattern features on a part file with a part copy feature
PR 9390112: Part file will be deleted, if an assembly will not be saved
PR 9421254: Solid Edge rashes when trying save the assembly each time (Has wire-harness)
PR 9203749 frames about "Extend/Trim a frame segment causes unexpected results."
PR 9428554: Changes to help address random crashes
PR 9444743: Fixed a reproducible crash captured in a submitted crashlog
PR 9233005: When IPA the locating of geometry outside of the IPA path was incorrect
PR 8407232 Parts cannot be deleted, if all parts are activated
PR 9242392: Solid Edge crashes while importing harness data using a specific workflow
===Draft=== PR 9284474 : Problem with Horizontal Break line for Broken View
===Part/Sheet Metal===PR 9409771: Solid Edge aborts when adding and editing custom material property
PR 9436802: The costumer made one .par via mirror component and cannot change the material
PR 9273919: Cannot edit the property Comments of Solid Edge documents in Windows Explorer
PR 8359548: Radial dimensions are not converted to driving (blue) with create 3D command
PR 8405442: Performance issue when material file is on a share
PR 9385673: When starting Solid Edge, it also tries to start Microsoft Excel, which crashes
PR 9402907: Stamp in Design for Cost does not recognize patterned occurrences
PR 9330034: Locate issues with small parts
PR 9433809: Text profile displays additional geometry with accelerated sketch
PR 9226405: Patterned helical cutout does not maintain correct distance between occurrences
PR 9382697: Reference plane is not staying in correct position
===Translators===PR 9143216: STEP file does not open correct, models missing
PR 8938269: SW2013 After the data is migrated, the configuration has no conversion
PR 9350279: When trying to bring NX file into SE, SE aborts
PR 9363120: Object Border set not shown is shown in DXF result
PR 9474274: SW2014 - Migrated drawings are not the same
PR 8989682: Open the step file in SE, the result is wrong and not complete
===Data Management===PR 9419705 : Impossible to replace parts located in a Solid Edge Data Management Standard Parts Folder
===Teamcenter Integration for Solid Edge===PR 9342842: Solid Edge crashes when editing a part
PR 9397514: Performance suffers on Teamcenter Tab
PR 9427010: Replace a new revision with an older revision
PR 9428205: Solid Edge crashed while doing Multi - body Publish
SFB-SOLID_EDGE-8014150
Product Information: