NX About the appearance of the shape in the case of Non-Geometric components in Structure manager.

2021-10-06T23:27:21Z
NX for Design

Summary


Details

Create an assembly with the components of the "Component is Non-Geometric" setting in NX.
The user can't see the shape in NX.
Now open this assembly in TC Vis.
The user can't see the shape in TC Vis.
But when you open the same assembly in Structure Manager you can see the shape or geometry even though it is a Non-Geometric component. The user wants to know how to avoid this in Structure Manager.





Solution

In the Structure Manager add a Colum "UG GEOMETRY" and set the value as "NO".
Then set the Preference "TCVIS_allow_NGC_expand" to False and Restart Teamcenter.
You will not see the geometry for the Non-Geometric component in Structure Manager.





Notes and References

IR#8556625

Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 2008_R2
Product: NX
Application: NXMANAGER
Version: V12.0.2
Function: FILE_SAVE

Ref: 002-8014132

KB Article ID# PL8014132

Contents

SummaryDetails

Associated Components

Teamcenter Integration for NX