NX Measure command does not allow for Feature creation when component is the Work Part

2021-10-06T23:27:21Z
NX for Design

Summary


Details

Unable to create geometry with the new Measure command while working in the context of an assembly.



Solution

Prior to NX12.0.2, the 'Measure' command would allow creation of geometry in the assembly when making a component the Work Part. However, this is no longer available. The component should be made the Displayed part so the 'Measure' command can be used with the 'Create Geometry' option.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DESIGN
Version: V1847
Function: INFO_ANALYSIS

Ref: 001-9488836

KB Article ID# PL8014131

Contents

SummaryDetails

Associated Components

Modeling