This error - "2705 Error Code" - is usually caused by some Windows Operating System misconfigured or damaged file(s).
We suggest you contact your IT Team and have them review some of the events listed below which may have caused this such as:
An incomplete installation
An incomplete uninstall
Improper deletion of applications or hardware
It can also be caused if your computer is recovered from a virus or adware/spyware attack or by an improper shutdown of the computer.
All the above actives may result in the deletion or corruption of entries in the Windows system registry. This corrupted registry will lead to the missing and incorrectly linked files needed for the proper working of the application.
Hardware/Software Configuration
Platform: INTL64 OS: windows OS Version: 2012_R2 Product: SOLID_EDGE Application: SETUP Version: V219MP4 Function: LICENSING