Manual text in NX1847

2021-10-06T23:27:21Z

Summary


Details

In Pre-NX1847, manual text could be entered in a drafting dimension using the command in the Menu, 'Edit > Annotation > Text'. 

In NX1847 and later versions, this command is not displayed.



Solution

This command is currently hidden but can be added back to the toolbars using the 'Customization' command.

1. Once in the Drafting application, in the Menu, select 'Tools-->Customize'
2. Under Categories, expand 'Menu-->Edit' and highlight 'Annotation'
3. Use the mouse to drag and drop the command 'Text (to be retired)...' back into the menus or ribbon toolbar to the desired location
4. Close the Customize dialog

Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DRAFTING
Version: V1847
Function: ANNOTATION

Ref: 002-8014120

KB Article ID# PL8014120

Contents

SummaryDetails

Associated Components